2601_MTN6705-0008S_MTN6805-0008_SW

Behavior at Pressed/Released

  • Blinking/relay opened

With pressed (telegram value “1”), the relay starts blinking. With released (telegram value “0” during blinking), the relay stops blinking and the relay is opened.


Blinking/relay opened


  • Blinking/relay closed

With pressed (telegram value “1”), the relay starts blinking. With released (telegram value “0” during blinking), the relay stops blinking and the relay is closed.


Blinking/relay closed


  • Relay opened/blinking

With pressed (telegram value “1”), the relay stops blinking and the relay is opened. With released (telegram value “0” during blinking), the relay starts blinking.

The blinking cycle starts with a closed relay immediately after the download. Following the download, the switch object is released.


Relay opened/blinking


  • Relay closed/blinking

With pressed (telegram value “1”), the relay stops blinking and the relay is closed. With released (telegram value “0” during blinking), the relay starts blinking.

The blinking cycle starts with a closed relay immediately after the download. Following the download, the switch object is released.


Relay closed/blinking

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?