Device Protection and Cyber Security
The SpaceLogic KNX Switch/Blind Master has a micro USB B interface. This is intended for diagnostic and updating the firmware of the device. A 4-digit PIN code should be set in the ETS application to prevent unauthorized persons from manipulating the firmware (Cyber Security).
This is requested before a firmware update with the Schneider Electric “Device Firmware Update Tool”. Without this PIN, an update is not possible. You have 3 attempts to enter a valid access code. If the code is not entered correctly, the service port is disabled for 1 hour or the device needs to be restarted (power reset or device reset).
|
General settings |
Device protection information: No valid PIN Code for Firmware Update! Please enter a valid PIN code in the extended settings before downloading your configuration! |
The PIN code is entered on the Extended settings tab (PIN Code for Firmware Update). Weak PINs are forbidden (e.g., 1234, 1111, 2222, ...).