2601_MTN6705-0008S_MTN6805-0008_SW

Activating Extended Settings for Blind/Roller Shutter

Master / Ext. 1/2

Output 1+2 / 3+4 / 5+6 / 7+8

-Blind/roller shutter

Express settings for blind/roller shutter

 

Extended settings for blind/roller shutter

No

Yes

To activate the extended settings for blind/roller shutter, you must enable them here.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?