2601_MTN6705-0008S_MTN6805-0008_SW

Same Running Times for Up and Down

Master / Ext. 1/2

Output 1+2 / 3+4 / 5+6 / 7+8

Blind/roller shutter

Express settings for blind/roller shutter

 

Blind control / roller shutter control

 

Use same time for up and down

Yes

 

Up/Down time (5s...99:59.9 min)

02:00.0

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?