2601_MTN6705-0008S_MTN6805-0008_SW

Reference Movement with Movement Range Limitation

NOTICE
Blinds/roller shutters can be damaged.
  • The blinds/roller shutters may move outside the movement range limits and into any open windows. For this reason, consider where the reference movement is to be made (Calibration).
  • After a download or bus voltage recovery, a reference movement is made after initialization, even if the General reference movement function is disabled. The blinds/roller shutters may move outside the movement range limits and into any open windows. (Calibration).
  • After a download or bus voltage recovery, the movement range limitation may be disabled because no activation telegram has been received.
  • For this reason, consider where the reference movement is to be made: The reference movement after initialization is generally carried out towards the upper end position. A reference movement to the lower end position is only carried out if the parameter Reference position is set to lower.
  • Functions with a higher priority, such as safety function or alarm function, can also control blinds/roller shutters outside the movement range limitation.

Movement Range Limits

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?