2601_MTN6705-0008S_MTN6805-0008_SW

Blind Type: Downwards Tilted/Upwards Horizontal

(With operating position)

  • Upward movement:
    Slats in horizontal open position (slat position 0%)

  • Downward movement:
    Slats tilted down in the operating position (slat position in operating position)

  • Possible adjustment range for the opening angle of the slats:
    0% to the operating position if blind not in lower end position
    0-100% if blind in lower end position


Downwards tilted/Upwards horizontal


The parameter Slat position after movement in % allows you to define the behavior of the slats after a movement for the channel.

Master / Ext. 1/2

Output 1+2 / 3+4 / 5+6 / 7+8

Blind

Express settings for blind

 

Slat control

 

Movement of the existing blind

Downwards tilted / upwards horizontal

Slat position after movement in %

Last slat position

   

No reaction

   

Operating position

   

Existing slat position during downwards movement in %

50

You can use the parameter Existing slat position during downwards movement in % to set the opening angle for the operating position.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?