2601_MTN6705-0008S_MTN6805-0008_SW

Status of Moving

The status object “Feedback for moving” sends the movement status of the drive. This information is sent directly.

  • Sends a “1” when the movement/drive is started

  • Sends a “0” when the movement/drive is stopped

The status object “Feedback for last direction” sends the value for the last direction of movement of the drive.

  • Sends a “1” if the drive has been moved down or the slat has been closed by one step

  • Sends a “0” if the drive has been moved up or the slat has been opened by one step

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?