2601_MTN6705-0008S_MTN6805-0008_SW

Trigger of Calibration

Master / Ext. 1/2

Output 1+2 / 3+4 / 5+6 / 7+8

-Blind/roller shutter

Calibration

-Automatic, Locking & Calibration settings

Trigger of calibration

Number of movements

Value "1" on calibration object

No. of movements or calibration object

   

Delay of calibration via object (0...255, unit = 1 s)

0

   

Number of movements until calibration

7 (1-20)

Triggering a reference movement after a number of movements

The channel adds up the total number of movements, irrespective of the control command that triggered the movements. Once the defined number of movements has been reached, the drive first performs a reference movement before the next positioning command. It then moves to the requested position. After the reference movement, the movement counter is reset.


Trigger reference movement via group object

If the object "" receives the value "1", a reference movement is started for all assigned channels. In order not to overload the power supply of the blind system, you can select a "" for each channel. If a new value "1" is received on the object during this delay time, the delay time is restarted. The object value "0" has no meaning.


Trigger reference movement after a number of movements or via group object

It is also possible to select a logic operation from the number of movements or the calibration telegram.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?