2601_MTN6705-0008S_MTN6805-0008_SW

Locking Manual Mode

You can control the connected drives via the group objects the for manual operating options or via automatic control. There are two options available for the manual operating options:

  • Move manually to height position and slat opening angle (for blind only) via Up/Down/Step/Stop commands

  • Move manually to height position and slat opening angle (for blind only) using absolute position commands

If you want to stop manual operation temporarily, you can enable lock of manual mode for each output channel:

Master / Ext. 1/2

Output 1+2 / 3+4 / 5+6 / 7+8

Blind/roller shutter

Express settings for blind/roller shutter

 

Locking manual mode

Disabled

 

Enabled

Manual locking

At object value "1"

   

At object value "0"

Depending on the setting, manual operation is disabled or enabled when a new telegram value is received:

  • Manual locking” = “at object value “0”
    If “Manual locking” = “0”: manual operation disabled (manual locking active)
    If Manual locking = “1”: manual operation enabled (manual locking inactive)

  • Manual locking” = “at object value “1”
    If “Manual locking” = “0”: manual operation enabled (manual locking inactive)
    If “Manual locking” = “1”: manual operation disabled (manual locking active)

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?