2601_MTN6705-0008S_MTN6805-0008_SW

Drive Behavior after End of Weather Alarm

Once the sensor values of the weather sensors have returned to the normal measuring range, the weather alarms are deactivated again. You can define a reaction to be performed by the drive as soon as there is no longer any weather alarm active:

Master / Ext. 1/2

Output 1+2 / 3+4 / 5+6 / 7+8

-Blind / roller shutter

-Safety and alarm settings

Weather alarm function

Behavior at end of all weather alarms

No reaction

Up

Down

Move to position prior weather alarm

Accept current automatic position

The drive then performs the following functions:

  • No reaction: the drive remains in its current position. The alarm function is terminated.

  • Up: the drive moves to the upper end position. The alarm function is terminated.

  • Down: the drive moves to the lower end position. The alarm function is terminated.

  • Move to position prior weather alarm: the drive returns to the position it had before the weather alarm. The alarm function is terminated.

  • Accept current automatic position: this setting is only useful if the automatic function is active. The drive moves to the last automatic position requested. The alarm function is terminated.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?