2601_MTN6705-0008S_MTN6805-0008_SW

Central Function Delay Times

The delay times for all channels together are parameterized on the Extended settings tab.

Extended settings

Delay of central functions all channels (0...255, unit = 100ms)

0

 

Time between central functions per channel (2...255, unit = 100 ms)

5

The central function has the same priority as the normal switching function. Receiving a new object value via the central object has the same effect as receiving a new object value for the switch object of the output.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?