2601_MTN6705-0008S_MTN6805-0008_SW

Enabling Central Functions

The central function allows you to switch multiple output switching channels simultaneously with a telegram via the Central - Switch object.

This functionality is available, for example, if you want to switch off all lamps at the press of a button when leaving the house and switch on all lamps at the press of a button when cleaning the house or in the event of an alarm.


Decentralized control without central function:


Centralized control with central function:

For blinds and roller shutters, there is a separate central object with a corresponding central object.


In order to use the central function for the individual switch/blind/roller shutter channels, you must first enable the global function on the General settings tab.

General settings

Central functions

Disabled

   

Enabled

   

Enabled/Delayed

Following enabling, the group objects appear and all outputs are enabled for the central function.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?