2601_MTN6705-0008S_MTN6805-0008_SW

Lock Behavior after Bus Voltage Recovery

Disabled:
The locking function is not activated after a bus voltage recovery, regardless of the state it had before the bus voltage failure.


Enabled:
After a bus voltage recovery, the locking function becomes active and the output is switched to the state that you defined via the parameter Behavior at start of locking. If you have set the value No reaction here, the output is locked in its current state.


As before bus voltage failure:
The locking function is brought to the state that was active before the bus voltage failure. If the locking function was active, the output is controlled by its settings in the parameter Behavior at start of locking.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?