2601_MTN6705-0008S_MTN6805-0008_SW

Switching Cycle Counter

If you enable Switching cycle counter, all switching actions of a relay are counted and stored persistently in the memory. The actual value can be read for each relay via a 2-byte Switching cycle counter group object.

By default, only C-Flag and R-Flag are set to avoid high bus traffic. The firmware checks the internal counters cyclically every 10 seconds. If the value changes, it is sent via the group object.

You can read the actual values via group objects. If you want to get to know the values without reading, you have to set the T-Flag for the object.

You have to enable the visibility of group objects in “Extended settings” for the device. You can enable the visibility separately for each device (Master and Extensions).

Extended settings

Switching cycle counter

 

Master switching cycle counter

Disabled/Enabled

 

Extension 1 switching cycle counter

Disabled/Enabled

 

Extension 2 switching cycle counter

Disabled/Enabled

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?