2601_MTN6705-0008S_MTN6805-0008_SW

Global Settings for Feedback

Here you can set the delay of the feedback of this device and the time interval between multiple feedback telegrams.

If there is only one telegram to be sent, it is sent as set in the parameter Delay of status response for all channels. If more than one response is active, the other responses will be sent at the delay time intervals set by the parameter Time between responses per channel.



Extended settings

Global settings for feedback

 
 

Delay of status response for all channels (0...255, unit = 100 ms)

0

 

Time between status response per channel. (0...50, unit = 100 ms)

0

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?