2601_MTN6705-0008S_MTN6805-0008_SW

Suspend Manual Operation Automatically

You can set a time limit for manual operation when toggling to it. To do so, set the parameter Suspend manual operation automatically to Yes

Then set the parameter Suspend manual operation after 1...48 in hours to the desired time after which the device automatically resets manual operation. You can read the current operating status from the manual operation LED and you will receive feedback via the Status of manual operation object if you have enabled this function.

Extended settings

Manual operation settings

 

Suspend manual operation automatically

No

 

Yes

Suspend manual operation after (1...48, unit = 1 hour)

2

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?