2601_MTN6705-0008S_MTN6805-0008_SW

Calibration

The calibrating function is activated centrally on the Global settings for roller shutter and blind tab with the parameter Calibration.

See Calibration and Group Object for Calibration.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?