2601_MTN6705-0008S_MTN6805-0008_SW

Activating Extended Settings for Roller Shutter

To activate the extended settings for roller shutter, you must enable them here.

Master / Ext. 1/2

Output 1+2 / 3+4 / 5+6 / 7+8

-Roller shutter

Express settings for roller shutter

 

Extended settings for roller shutter

No

Yes

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?