2601_MTN6705-0008S_MTN6805-0008_SW

Group Objects of Automatic Mode Lock

No.

Name

Object function

Length

Behavior

Data Type

64

Master Output 1+2 name of the channel

Lock of automatic mode

1 bit

Received

1.003 Enable

72

Master Output 1+2 name of the channel

Feedback for automatic mode

1 bit

Sending

1.003 Enable

Depending on the setting, the automatic locking is activated or deactivated when a new telegram value is received:

  • Automatic locking” = “at object value 0
    If “Automatic locking” = “0”: automatic locking is active.
    If “Automatic locking” = “1”: automatic locking is inactive.

  • Automatic locking” = “at object value 1
    If “Automatic locking” = “0”: automatic locking is inactive.
    If “Automatic locking” = “1”: automatic locking is active.

In addition, you can set the behavior of the drive to the end of automatic locking.

Furthermore, you can separately define the response of automatic control on receiving a manual control telegram.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?