2601_MTN6705-0008S_MTN6805-0008_SW

Channel Name

You can assign a separate name for each channel, e.g. "Blind Kitchen". The name of the channel now appears on the parameters, channels and associated group objects.

Master / Ext. 1/2

Output 1+2 / 3+4 / 5+6 / 7+8

Blind/roller shutter

Express settings for blind/roller shutter

 
 

Name of the channel

Blind Kitchen

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?