2601_MTN6705-0008S_MTN6805-0008_SW

Automatic Mode

In addition to manual control of the blind / roller shutter drives (via the group objects for the manual operating options), the software application also provides you with another set of group objects for automatic control.

Automatic control can be performed by other bus devices, e.g. presence detectors or light controllers, or via a building control system. Once you have activated automatic control for a channel, you can initially position the connected drive with equal priority using manual control or automatic control. The drive reacts identically on receiving control telegrams from one of the two types of control.

Master / Ext. 1/2

Output 1+2 / 3+4 / 5+6 / 7+8

-Blind/roller shutter

Automatic, Locking & Calibration settings

-Automatic, Locking & Calibration settings

Automatic mode

   

Automatic mode

Disabled

Enabled

In order to use the automatic mode, you must first activate the function in the ETS. Once automatic mode has been enabled, new group objects are available for the channel.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?