2601_MTN6705-0008S_MTN6805-0008_SW

Priority

The scene function has the same priority as the normal blind / roller shutter function with control over the 4 group objects:

Movement in manual mode” and “Stop/step in manual mode” (for roller shutters: “Stop in manual mode”)

For positioning: “Height position in manual mode” and “Slat position in manual mode” (for blind only).


This should be taken into account with regard to the priority of the higher-level functions.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?