2601_MTN6705-0008S_MTN6805-0008_SW

Defining Channel Functions

Each output can be operated in the function disabled or switch or blind or roller shutter. In blind and roller shutter operation, two outputs are grouped together to form a single channel. The output contacts of the relays are then electronically interlocked. This means that you cannot switch on both contacts of a motor channel simultaneously. This applies to control via bus telegrams and to manual operation on the device.

NOTICE
Check before commissioning:
The load connections and the order of the devices (Master > Extension 1 > Extension 2) must correspond to your ETS programming.
  • Connect blind motors to the blind channels specified in the ETS.
  • Connect loads to the switching channels specified in the ETS.
  • If the extension is planned as extension 1 (E1), connect it directly to the master.
  • If the extension is planned as extension 2 (E2), then connect it to extension 1.
An extension cannot be put into operation if the order of the devices does not correspond to your programming in the ETS.

General settings

Channel function for master
 

Output 1-8

Disable

    Switch
     

Roller shutter

     

Blind

After activation of Extension 1

General settings

Channel function for Extension 1
 

Output 1-8

Disable

    Switch
     

Roller shutter

     

Blind

After activation of Extension 2

General settings

Channel function for Extension 2
 

Output 1-8

Disable

    Switch
     

Roller shutter

     

Blind

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?