2601_MTN6705-0008S_MTN6805-0008_SW

Behavior After Bus Voltage Recovery

Using the parameter Behavior after bus voltage recovery, you can define the reaction of the channel to bus voltage recovery and the switching state:


Disabled
Priority remains deactivated. The switching state of the channel results from the other higher-level functions or from the set switching behavior after bus voltage recovery.


Enabled, released
The priority is automatically activated on bus voltage recovery and the switching state is switched to Released.


Enabled, pressed
The priority is automatically activated on bus voltage recovery and the switching state is switched to Pressed.


As before bus voltage failure
The priority is brought to the state it had before the bus voltage failure. If the priority was previously active, the output relay is switched to the state it had previously.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?