2601_MTN6705-0008S_MTN6805-0008_SW

Switching

You can choose between the switching modes Switching and Blinking. In Switching mode, the relay opens and closes depending on the KNX telegram and the setting for the contact mode.

Master/Ext. 1/2 Output 1-8 -Switch: Switching

Express settings for switching

 
 

Switching mode

Switching

Blinking

 

Contact mode

Normally opened

Normally closed

The settings for Output 1 are described below, but apply equally to all outputs.

If you select switching mode Switching for output 1 on the master, an ETS channel with the name Master Output 1 - Switch +Name of the channel will be created. All the group objects for this output are located there.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?