2601_MTN6705-0008S_MTN6805-0008_SW

Lock Behavior after Download

After a download, the lock function is also set as in the case of bus voltage recovery. The parameter Behavior after download determines which state is set.

If the parameter Behavior after download is set to the value As before download, the locking function is activated as before and the relay is switched accordingly.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?