2601_MTN6705-0008S_MTN6805-0008_SW

Cyclic Sending Live Signal

With the setting Cyclic sending live signal > 0, the central sign of life object is activated (live signal).

If activated, the device cyclically sends the value “1” with the cycle time set. This information is only a sign of life from the KNX master. Here, for example, the device can be monitored in a visualization.

Extended settings

Device health

 
 

Cyclic sending live signal (0...255, unit = 1 s, 0 = inactive)

0

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?