2601_MTN6705-0008S_MTN6805-0008_SW

Behavior after Download

After the ETS download, the relay can adopt a parameterized state.

If an internal defect or a faulty download results in a state in which the application is not operational, the device will not react. The output relays remain in their last position.

If you wish to activate the behavior after ETS download for an output channel, you must select a “relay state at end of download” for each channel.


Possible settings:


As before download:
The relays execute the behavior set before the download. Any subsequent manual switching is overwritten. If a higher-level function (logic operation, priority control or lock) is active, the behavior you defined for these functions will be executed.


Pressed:
In the case of a normally opened contact, the relay is closed; in the case of a normally closed contact, the relay is opened.


Released:
In the case of a normally opened contact, the relay is opened; in the case of a normally closed contact, the relay is closed.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?