2601_MTN6705-0008S_MTN6805-0008_SW

Failure and Download Behavior

Failure and Download Behavior

Master / Ext. 1/2

Output 1+2 / 3+4 / 5+6 / 7+8

-Blind / roller shutter

-Safety and alarm settings

Failure and download behavior

Failure and download behavior

Disabled

Enabled

Relay state after bus voltage failure

No reaction

Stop

Up

Down

Relay state after bus voltage recovery

Stop

Up

Down

Move to position

As before bus voltage failure

   

Height position at bus voltage recovery in %

0 (0-100)

   

Slat position at bus voltage recovery in %

0 (0-100)

   

Relay state at end of download

Stop

Up

Down

Move to position

As before download

   

Height position at end of download in %

0 (0-100)

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?