MTN6705-0008S / MTN6805-0008

Components and Programming Environment

The device is commissioned using KNX-certified software. The application and the technical descriptions are updated regularly and can be found on the Internet. This application runs in conjunction with ETS software version 5 or higher.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?