2601_MTN6705-0008S_MTN6805-0008_SW

Activation of Manual Operation

Manual operation can be disabled on the device in the ETS. This means that operation on the device is no longer possible.

Extended settings

Manual operation settings

 

Activation of manual operation on the device is

Not allowed

   

Allowed

Manual operation is allowed as a standard.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?