2601_MTN6705-0008S_MTN6805-0008_SW

Priority of Weather Alarms

The global priorities for the weather alarms are defined here.

Extended settings

Global settings for roller shutter and blind

 

Priority of weather alarms

Wind alarm >Rain alarm >Frost alarm

 

Wind alarm > Frost alarm > Rain alarm

Monitoring time for wind alarm 1

Rain alarm > Wind alarm > Frost alarm

   

Rain alarm > Frost alarm > Wind alarm

 

Monitoring time for wind alarm 2

Frost alarm > Rain alarm > Wind alarm

     

Frost alarm > Wind alarm > Rain alarm

This priority setting applies to all blind and roller shutter channels for which the weather alarm function is enabled. The reactions to a weather alarm only become active if no weather alarm with a higher priority is already active. If a weather alarm is reset and another weather alarm with a lower priority is active at that time, the reactions of the alarm with the lower priority are now executed.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?