2601_MTN6705-0008S_MTN6805-0008_SW

Alarm Function

In the case of an alarm, the alarm function can be used to set each output to a desired alarm state. The output is disabled for further operation. Only a higher-level function with a higher priority can still be used to switch the output to a different state. You can activate the alarm function individually for each output channel. The alarm function can be parameterized here for each channel.

Master/Ext. 1/2 Output 1-8 -Switch: Switching

Alarm function

 
– Safety and alarm settings

Alarm function

Disabled

Enabled

 

Alarm

At object value "1"

At object value "0"

   

Behavior at start of alarm

No reaction

Pressed

Released

Blinking (5s cycle)

   

Behavior at end of alarm

No reaction

Pressed

Released

Follows current value

   

Behavior after bus voltage recovery

Disabled

Enabled

As before bus voltage failure

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?