Operating ETS Software
Essential Skills for ETS Operation in KNX Systems
To operate the ETS software application, you need the following skills:
-
Basic Windows operation: Understanding the basic rules for operating programs using Windows is essential.
-
ETS software knowledge: Familiarity with the ETS software, including how to navigate its interface and use its features.
-
KNX system understanding: Knowledge of the KNX system, including how to select the correct sensors and actuators, transfer them to the line, and commission them.
-
Programming skills: Ability to program the KNX push button, which involves setting parameters, assigning group addresses, and configuring functions
ETS Parameter Settings and User Interface Overview
Tables with describe parameter settings in ETS.
In the ETS, the device parameters are opened using the Parameters tab.
The user interface is divided into 2 sections: The tabs are on the left and the parameters on the right, together with their values.