2601_MTN6705-0008S_MTN6805-0008_SW

Extended Settings for Roller Shutter

Extended Settings for Blind/Roller Shutter

Master / Ext. 1/2

Output 1+2 / 3+4 / 5+6 / 7+8

-Blind/roller shutter

Express settings for blind/roller shutter

Extended settings for blind/roller shutter

No

Yes

 

-Extended drive timing

Idle time until upward movement

 
   

Startup delay

 
   

Additional startup time

 
 

-Automatic, Locking & Calibration settings

Priority function

 
   

Logic function

 
 

-Safety and alarm settings

Safety function

 
   

Alarm function

 
   

Failure and download behavior

 

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?