2601_MTN6705-0008S_MTN6805-0008_SW

Group Objects of the Move Range Limits Function

No.

Name

Object function

Length

Behavior

Data Type

68

Master Output 1+2 name of the channel

Activate movement range limits

1 bit

Received

1.003 Enable

74

Master Output 1+2 name of the channel

Feedback for range limitation

1 bit

Sending

1.003 Enable

In addition, a status feedback object can be enabled that sends the status of the movement range limits function to the bus.

The value of the status feedback object receives the object value "1" as soon as the movement range limitation becomes active and the drive reaches the specified limit.

  • If the drive is already within the specified limit when the movement range limitation is activated, the status feedback object immediately sends the object value "1".

  • If the movement range is left or the limit is canceled due to a function with a higher priority, the object value changes to "0".

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?