2601_MTN6705-0008S_MTN6805-0008_SW

XOR Logic Operation

As soon as the values of the “logic object” and the “switch object” differ from one another, the output is switched to Pressed. If the values are the same, the output is Released.

Object Logical input

Object Switching

Result

0

0

0

0

1

1

1

0

1

1

1

0

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?