2601_MTN6705-0008S_MTN6805-0008_SW

Enable Button for Manual Operation via Object

Switching to manual operation control via the Manual push-button is only possible if the object Enable button for manual operation via object has the value “1”. If the object has the value “0”, toggling to manual operation is disabled. If toggling is disabled by a telegram, the device also automatically deactivates manual operation.

The value of the object Enable button for manual operation via object can be parameterized after bus voltage recovery. The value “1” enables the Manual push-button and the outputs can be operated on the device. The value “0” disables the Manual push-button after bus voltage recovery.

Extended settings

Manual operation settings

 

Enable button for manual operation via object

No

 

Yes

Object value after bus voltage recovery

0 (Manual push-button disabled)

   

1 (Manual push-button enabled)

   

As before bus voltage failure

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?