Overview of Application Functions
|
Central functions |
Disabled Enabled Enabled/Delayed |
|
Select SpaceLogic KNX Extensions 1 and 2 |
MTN6805-0008 Switch/Blind |
|
Select channel functions of the master/extensions for each output |
Disabled Switch Roller shutter Blind |
|
Energy saving |
LEDs on the device can be set to standby after (0...255, unit = 1 min, 0 = always on) |
|
Device safety |
Disabled At object value “1” At object value “0” |
|
Device health |
Cyclic sending live signal Enable outputs for failure indication |
|
Switching cycle counter |
Master/Extension 1/2 switching cycle counter (Disabled/Enabled |
|
Global settings for scene |
Naming of the scenes Enable learning of scenes Enable description text field for scenes |
|
Delay for central functions (Only if central function is enabled with delay) |
Delay of central functions all channels Time between central functions per channel |
|
Global settings for feedback |
Delay of status response for all channels Time between status response per channel |
|
Sending delay |
Sending delay after bus voltage recovery |
|
Manual operation settings |
Activation of manual operation on the device is not allowed/allowed Enable button for manual operation via object Suspend manual operation automatically Send status of manual operation via object |
|
Global settings for switching |
Collected status response Priority of functions |
|
Global settings for roller shutter and blind |
Weather alarm functions Priority of functions Calibration |
|
PIN Code for Firmware Update via USB |
Enter a PIN code for firmware update. |
|
Device information |
Firmware Master Firmware Extension 1/2 Uptime Master (days/hours/min/sec) |
|
Name of the channel |
|
|
Switching mode |
Switching/Blinking |
|
Contact mode |
Normally opened/closed |
|
Operating hours counter |
Disabled/Enabled |
|
Scenes |
Disabled/Enabled |
|
Central function |
Disabled/Enabled |
|
Status response |
Normal behavior/Inverted |
|
Extended settings for switching |
|
|
Scene settings (if Scenes function in Express settings is enabled) |
Required number of scenes Overwrite scene values in actuator during download Time delay for scene processing Scene Nr.
|
|
Time settings |
Staircase lighting time On-delay time Off-delay time |
|
Logic, Locking & Priority settings |
Priority function Logic function |
|
Safety and alarm settings |
Safety function (if Device safety in Extended settings is enabled) Alarm function Failure and download behavior |
|
Name of the channel |
|
|
Blind/Roller shutter control |
Use same time for up and down Up/Down time (same or different) Pause time before reverting |
|
Slat control |
Slat rotation time Steps that shall be executed during slat rotation Movement of the existing blind Slat position after movement in % |
|
Lock of manual mode |
Disabled/Enabled |
|
Scenes |
Disabled/Enabled |
|
Central function |
Disabled/Enabled |
|
Status of height |
Disabled/Enabled |
|
Status of slat |
Disabled/Enabled |
|
Status of moving |
Disabled/Enabled |
|
Extended settings for blind/roller shutter |
|
|
Scene settings (if Scenes function in Express settings is enabled) |
Required number of scenes Overwrite scene values in actuator during download Time delay for scene processing Scene Nr.
|
|
Extended drive timing |
Idle time until upward movement Startup delay Deceleration delay Additional startup time when opening slat upwards/downwards |
|
Automatic, Locking & Calibration settings |
Automatic mode Locking function Movement range limits Calibration |
|
Safety and alarm settings |
Safety function (if Device safety in Extended settings is enabled) Alarm function Weather alarm (if Weather alarm is enabled in Extended settings) Failure and download behavior |