2601_MTN6705-0008S_MTN6805-0008_SW

Device Safety

This parameter activates the central safety object.

For each channel, a channel parameter can be used to determine whether and how this channel should respond to the safety object. The object value for the device safety function can also be set.

The device then waits for a telegram from an external sender within the set cycle time. If such a telegram is not received within the monitoring time, it is then possible to decide for each channel what should happen.

Switch: Safety Function Switching

Blind: Safety Function for Blind

Roller shutter: Safety Function for Roller Shutter

Extended settings

Device safety

 
 

Device safety

At object value "1"

     

At object value "0"

     

Disabled

   

Cycle time surveillance for Safety object (0 ... 255, unit = 1 s, 0 = inactive)

0

After enabling device safety function, the Safety group object appears.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?