MTN6705-0008S / MTN6805-0008

Group Object for Calibration

No.

Name

Object function

Length

Behavior

Data Type

17

Central

Calibration

1 bit

Received

1.010 Start/Stop

The channel-specific settings for the calibrating function can be found in Calibration.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?