2601_MTN6705-0008S_MTN6805-0008_SW

Group Objects of Status Response of Roller Shutter

No.

Name

Object function

Length

Behavior

Data Type

70

Master Output 1+2 name of the channel

Feedback for height

1 byte

Sending

5.001 Percent (0...100%)

75

Master Output 1+2 name of the channel

Feedback for moving

1 bit

Sending

1.010 Start/Stop

76

Master Output 1+2 name of the channel

Feedback for last direction

1 bit

Sending

1.008 Up/DOWN

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?