2601_MTN6705-0008S_MTN6805-0008_SW

Status Response

Depending on the parameterization, each channel can return a status response. The following parameter settings are available for this:

Normal behavior (Pressed = 1; Released = 0)

Inverted (Pressed = 0; Released = 1)

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?