2601_MTN6705-0008S_MTN6805-0008_SW

Time Delay for Scene Processing

To avoid high power-on currents when switching to a complex scene, you can parameterize a time delay for each output channel. (Especially in the case of many motors).

Master / Ext. 1/2

Output 1+2 / 3+4 / 5+6 / 7+8

-Blind / roller shutter

Scene settings

 
Scenes settings

Time delay for scene processing (0...255, unit = 100 ms)

0

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?