Group Objects of Status Response of Automatic Mode
|
No. |
Name |
Object function |
Length |
Behavior |
Data Type |
|---|---|---|---|---|---|
|
72 |
Master Output 1+2 name of the channel |
Feedback for automatic mode |
1 bit |
Sending |
1.003 Enable |
The feedback object sends a "1" if automatic locking is active.
The feedback object sends a "0" if automatic locking is inactive.