2601_MTN6705-0008S_MTN6805-0008_SW

Number of Scenes

Master / Ext. 1/2

Output 1+2 / 3+4 / 5+6 / 7+8

-Blind / roller shutter

Scene settings

 

Scenes settings

Required number of scenes

1 (1 – 16)

You can use the scene function to include multiple channels in a scene control. Up to 16 different scenes are available for each output channel.

Each of the 16 scenes can be disabled again.

Master / Ext. 1/2

Output 1+2 / 3+4 / 5+6 / 7+8

-Blind / roller shutter

Scene settings

 

Scenes settings

Scene 1 (1-16)

Disabled

Enabled

   

Scene 1 Description

   

Scene 1 Address (0-63)

Dependent: Global Settings for Scenes

Scene address 0 - 63

   

Scene 1 Address (1-64)

Dependent: Global Settings for Scenes

Scene address 1 - 64

   

Scene 1 height in %

0 (0-100)

   

Scene 1 slat position in %

0 (0-100)

For clarity, a short description can be stored for each scene.

Each of these scenes can be assigned one of 64 possible scene addresses 0 to 63 (corresponding to telegram values 0-63) or 1 to 64 (corresponding to telegram values 0-63). This depends on the global settings for scenes.

Global Settings for Scenes


You can store height positions and also, for blinds, slat opening angles as scene values. When the actuator receives a telegram calling a scene number, the drive is moved to the saved position and the slats are rotated. The scene positions you store during start-up can be overwritten later by the user if he wants to change them.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?