Express Settings for Blind/Roller Shutter
On the Express settings for blind / roller shutter tab, you can set basic settings and enable or disable other functions.
To control blinds/roller shutters, you can set the channel function of the device to the operating mode Blind or roller shutter. Now, two outputs will always be merged into a single blind / roller shutter channel. Please install the drives according to the installation instructions.
The operating mode is selected for each output on the Defining Channel Functions:
|
General settings |
Channel function for Master / Extension 1 / Extension 2 Output 1+2 / 3+4 / 5+6 / 7+8 |
Blind |
|
|
Master / Ext. 1/2 Output 1+2 / 3+4 / 5+6 / 7+8 Blind |
Express settings for blind |
... |
Please install the drives according to the installation instructions. When connecting the motor, note the correct direction of rotation for movement up/down.
There are many different blind variants for indoor and outdoor use. The channel enables the control of a blind / roller shutter motor with max. 1000 VA. Only one motor may be connected per channel. The motor must have an end position switch.