2601_MTN6705-0008S_MTN6805-0008_SW

Behavior after Download

After the ETS download, the channel can adopt a parameterized state. If an internal defect or a faulty download results in a state in which the application is not operational, the device will not react. The output relays remain in their last position.

If you wish to activate the behavior after ETS download for a drive, you must parameterize a “relay state at end of download” for each channel.


Possible settings:

  • Stop: the drive stops immediately.

  • Up: the drive moves to the upper end position.

  • Down: the drive moves to the lower end position.

  • Move to position: the drive moves to the defined position for height and slat (for blind only).

  • As before download: the drive remains in its current state after a download.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?