2601_MTN6705-0008S_MTN6805-0008_SW

Central Function for Switching

The central function is enabled or disabled here for each switch output.

Master/Ext. 1/2 Output 1-8 -Switch: Switching

Express settings for switching

 
 

Central function

Enabled

Disabled

The global settings and explanations of the central function can be found in the chapter Enabling Central Functions.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?