2601_MTN6705-0008S_MTN6805-0008_SW

Group Objects of Locking Function

No.

Name

Object function

Length

Behavior

Data Type

65

Master Output 1+2 name of the channel

Lock

1 bit

Received

1.003 Enable

73

Master Output 1+2 name of the channel

Feedback for drive locking

1 bit

Sending

1.003 Enable

If the locking object receives a telegram with the object value that you set for the parameter Lock, all other functions for the channel are disabled. You can define the reaction using the parameter Behavior at start of locking.

If the locking object receives a telegram with the object value opposite of that for activation, the lock is canceled and the drive adopts the state that you defined in the parameter Behavior at end of locking.

The Feedback for drive locking object sends a “1” if the lock is active.

The Feedback for drive locking object sends a “0” if the lock is inactive.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?